Modes of operation display
| Index.Sub | 6061.0H | ||||||||||||||||||||||
| Data Type | Integer8 | ||||||||||||||||||||||
| Access | Read Only | ||||||||||||||||||||||
| PDO Mappable | TX_PDO (1) | ||||||||||||||||||||||
| Unit | -- | ||||||||||||||||||||||
|
Range |
9 | ||||||||||||||||||||||
| Default Value | No | ||||||||||||||||||||||
| Store Supported | No | ||||||||||||||||||||||
| Description |
This parameter shows the current mode of operation. The meaning of the returned value corresponds to that of the modes of operation Modes of operation6060.0H).
|
||||||||||||||||||||||
|
Notes |
(1) available with firmware V00r74 or superior. (2) available with firmware V03r03 or superior. (3) available with firmware V03r21 or superior. |